earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Commission, IP-IO , MP-C, MP-V, RP-C
Functionalities: Engineering, BACnet/IP devices
Product version: 3.3, 2022, 2023, 2024
7/19/2021

Preparations

Prior to using the eCommission SmartX Controllers mobile application at a job site, there are some preparations you must make to facilitate device commissioning.

For more information, see Commission Mobile Application Overview .

Launching and Activating the eCommission Application

You launch and then activate the eCommission SmartX Controllers mobile application to create an account before you can perform any tasks.

Downloading and Starting the eCommission Application

You download and start the eCommission SmartX Controllers mobile application to perform commissioning, flow balance, and checkout operations on BACnet/IP controllers.

For more information, see Downloading and Starting the eCommission SmartX Controllers Mobile Application .

Transferring an Application Image File to a Mobile Device

Image files are created by a WorkStation user and contain pre-engineered objects, properties, and values. Download an Image to a BACnet/IP controller to facilitate device commissioning tasks.

For more information, see Image Downloading .

  • Commission Mobile Application Overview
  • Downloading and Starting the eCommission SmartX Controllers Mobile Application
  • Transferring an Application Image File