earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interfaz de usuario

Interfaz de usuario


Productos IP-IO , MP-C
Funcionalidades: Hardware
Versión del producto: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023, 2024, 7.0
13/03/2019

About Screen on MP-C or IP-IO Module

Use the About screen to get information on the firmware for the MP-C or IP-IO module I/O CPU and main CPU.

 
action_zoom_plus_stroke About screen on MP-C or IP-IO module
Figura: About screen on MP-C or IP-IO module

Tabla: About Screen on MP-C or IP-IO Module

Component

Description

IO Firmware:

[Version]

Displays the firmware version for the MP-C or IP-IO module I/O CPU.

CPU Firmware:

[Version]

Displays the firmware version for the MP-C or IP-IO module main CPU.

  • Configure Inputs and Outputs for Temporary Use