earth_america
user_standard Anmelden
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Konzept

Konzept


Produkte: AS-B, Edge Server, AS-P
Funktionen: Programmierung, Sicherheit
Produktversion: 2023, 2024, 7.0
03.12.2024

Disable Automation Server Ports

You can disable port 22 and the USB ports on the automation server.

Port 22

Port 22 is used for communication with Device Administrator. This port is often the target for cyber-attacks. You can disable this port or change the port so that the automation server communicates on another port using SSH. You can also disable all SSH communication.

Für weitere Informationen siehe Disabling Port 22 on an Automation Server .

Für weitere Informationen siehe Adding an Additional SSH Port for an automation Server .

USB port

To prevent anyone from tampering with your automation servers on site you can disable the USB ports.

The USB ports can be disabled on both the AS-B and AS-P servers but not on the automation server AS. The setting is visible on the automation server AS but grayed out and cannot be changed.

Für weitere Informationen siehe Disabling the USB Port on an Automation Server  .

  • Security Overview
  • Disabling Port 22 on an Automation Server
  • Adding an Additional SSH Port for an automation Server
  • Disabling the USB Port on an Automation Server