earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: AS-B, Edge Server, AS-P
Functionalities: Programming, Security
Product version: 2023, 2024
12/17/2022

Disable Automation Server Ports

You can disable port 22 and the USB ports on the automation server.

Port 22

Port 22 is used for communication with Device Administrator. This port is often the target for cyber-attacks. You can disable this port or change the port so that the automation server communicates on another port using SSH. You can also disable all SSH communication.

For more information, see Disabling Port 22 on an Automation Server .

For more information, see Adding an Additional SSH Port for an automation Server .

USB port

To prevent anyone from tampering with your automation servers on site you can disable the USB ports.

The USB ports can be disabled on both the AS-B and AS-P servers but not on the automation server AS. The setting is visible on the automation server AS but grayed out and cannot be changed.

For more information, see Disabling the USB Port on an Automation Server  .

  • Security Overview
  • Disabling Port 22 on an Automation Server
  • Adding an Additional SSH Port for an automation Server
  • Disabling the USB Port on an Automation Server