earth_america
user_standard Zaloguj się
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Pojęcie

Pojęcie


Produkty: AS-B, AS-P
Funkcje: Programowanie, Bezpieczeństwo
Wersja produktu: 3.3, 2022
2022-12-14

Disable Automation Server Ports

You can disable port 22 and the USB ports on the automation server.

Port 22

Port 22 is used for communication with Device Administrator. This port is often the target for cyber-attacks. You can disable this port or change the port so that the automation server communicates on another port using SSH. You can also disable all SSH communication.

Więcej informacji zawiera Disabling Port 22 on an Automation Server .

Więcej informacji zawiera Adding an Additional SSH Port for an automation Server .

USB port

To prevent anyone from tampering with your automation servers on site you can disable the USB ports.

The USB ports can be disabled on both the AS-B and AS-P servers but not on the automation server AS. The setting is visible on the automation server AS but grayed out and cannot be changed.

Więcej informacji zawiera Disabling the USB Port on an Automation Server  .

  • Security Overview
  • Disabling Port 22 on an Automation Server
  • Adding an Additional SSH Port for an automation Server
  • Disabling the USB Port on an Automation Server