earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Explicación de procesos

Explicación de procesos


Productos AS-B, AS-P
Funcionalidades: Programación, Seguridad
Versión del producto: 3.3, 2022, 2023, 2024
14/12/2022

Disabling the USB Port on an Automation Server 

To increase security, you disable the USB port on your AS-B server and AS-P server.

Mostrar más
action_close

You can disable port 22 and the USB ports on the automation server.

Port 22

Port 22 is used for communication with Device Administrator. This port is often the target for cyber-attacks. You can disable this port or change the port so that the automation server communicates on another port using SSH. You can also disable all SSH communication.

Para obtener más información, consulte Disabling Port 22 on an Automation Server .

Para obtener más información, consulte Adding an Additional SSH Port for an automation Server .

USB port

To prevent anyone from tampering with your automation servers on site you can disable the USB ports.

The USB ports can be disabled on both the AS-B and AS-P servers but not on the automation server AS. The setting is visible on the automation server AS but grayed out and cannot be changed.

Para obtener más información, consulte Disabling the USB Port on an Automation Server  .

To disable the USB Port on an automation server
  1. In WorkStation, in the System Tree pane, select the AS-B server or AS-P server.

  2. Click the Properties tab.

  3. Click the Network tab.

  4. Expand Port Settings .

  5. In the USB port box, select Disable .

  6. Click Save .

Aviso

You need to reset the automation server for the changes to take effect.

Para obtener más información, consulte Resetting a Automation Server .

  • Disable Automation Server Ports
  • Resetting a Automation Server