earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: SpaceLogic Sensor
Functionalities: 3-button, Hardware
Product version: 2.0, 2.1, 3.0, 3.1, 3.2
5/18/2018

Changing the Temperature Setpoint

In the SmartX Sensor 3-Button Cover mode, you change the temperature setpoint to increase living space comfort by using the available buttons. You enable the temperature setpoint by configuring the Display object Allow setpoint changes , followed by the Setpoint hig h limi t and Setpoint low limit properties. In this way, you can use the desired setpoint to control applications through the Setpoint property.

Show More
action_close

You use the SmartX Sensor Display property tabs in WorkStation to view and configure the UI features of the various sensor models within your control application.

Basic and Advanced Property Tabs

The Display Basic tab properties includes the same General Information you find on all EcoStruxure Building Operation objects. Beyond that, it also provides a Setpoint , a Fan speed , an Occupancy override , an HVAC mode , a Heating cooling status , and 4 Custom value text fields.

The Display Advanced property tab includes considerably more configuration information. For example, you enable the temperature setpoint feature by setting the Display object Allow setpoint changes property to On and configuring the Setpoint high limit and Setpoint low limit properties. If colored wall back lighting feedback is required for the room occupant, you can turn on the Enable wall back lighting property.

Note:

Allow setpoint changes, Setpoint high limit, and Setpoint low limit are the types of properties you may wish to drive dynamically based on time of day. For example, using a schedule, you may only allow setpoint changes during the day and not at night. You may also only change the high and low limits for the setpoint based on whether you are in the heating or cooling season.

You can also enable the occupancy override feature using the Display object Allow occupancy override property. In the Occupied mode, you then turn on a green back light if the Enable wall back lighting property is On .

For more information, see Configuring SmartX Sensor Display Properties .

Property Mapping

While the Display property tabs allow you to configure varied SmartX Sensor models with different UI features, not all of the properties apply to each model. Be sure to consider this when configuring the application and binding it to your control programs. The table that follows shows the properties applicable to each unit.

Table: SmartX Sensor and Display Object Property Mapping

Display property

Touchscreen Display

LCD Temperature Sensor

3-Button Cover

Setpoint

Yes

Yes

Yes

Fan speed

Yes

Yes

No

Occupancy override

Yes

Yes

Yes

HVAC mode

Yes

Yes

No

Heating cooling status

Yes

Yes

No

Show time

Yes

No

No

Time format

Yes

No

No

Show CO2

Yes

Yes

No

Show humidity

Yes

Yes

No

Temperature units

Yes

Yes

No

Allowed fan speeds

Yes

Yes

No

Enable wall back lighting

No

No

Yes

Allowed HVAC modes

Yes

Yes

No

Allow setpoint changes

Yes

Yes

Yes

Setpoint high limit

Yes

Yes

Yes

Setpoint low limit

Yes

Yes

Yes

Allow fan speed changes

Yes

Yes

No

Allow occupancy overrides

Yes

Yes

No

Allow HVAC mode changes

Yes

Yes

No

Allow menu pages

Yes

No

No

Allow HVAC mode changes

Yes

Yes

No

Allow menu page

Yes

No

No

Allow information pages

Yes

No

No

Allow temperature unit changes

Yes

Yes

No

Display backlight

Yes

No

No

SmartX Living Space Sensor / Eco mode

Yes

Yes

Yes

To change the temperature setpoint
  1. In the SmartX Sensor 3-Button Cover Model, press the

     
    action_zoom_plus_stroke
    button to increase the temperature setpoint in the designated living space.

  2. Press the

     
    action_zoom_plus_stroke
    button to decrease the temperature setpoint in the designated living space.

    Important:

    With each consecutive button push, the temperature setpoint increases or decreases by 10% within the specified setpoint range. The back light flashes quickly three time to indicate the top or bottom of range has been reached. Whenever possible, it is recommended that you set the range relatively narrowly (+/- 10 o ) to avoid wide temperature swings. With each button push, the back light also changes from deep blue at the low end of the range, to deep red at the top end of the range. For more information, see Backlighting in the SmartX Sensor 3-Button Cover Model .

  • SmartX Sensor Display Properties
  • Backlighting in the SmartX Sensor 3-Button Cover Model
  • SmartX Sensor 3-Button Cover Model
  • Configuring SmartX Sensor Display Properties