earth_america
user_standard Iniciar sessão
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Conceito

Conceito


Produtos: Device Administrator, License Administrator
Funcionalidades: Gestão de licenças
Versão do produto: 3.3, 2022, 2023, 2024
23-07-2021

EcoStruxure Building Operation Software Feature License Strings

The feature strings are used when you troubleshoot a license problem. The strings are visible in the Diagnostic tab of License Administrator.

Tabela: EcoStruxure Building Operation Software Feature License Strings

Product license

Feature string 1

Description

Client Station

client.station

Use this license to start and run WorkStation and WebStation.

Client tools

client.graphiceditor

client.script

client.functionblock.view

This license product group consists of several products, each required to run the corresponding client tool.

Licensing of WorkPlace Tech is included with the Script Editor license.

Enterprise Central

server.enterprise.central

Use this license to start and run an Enterprise Central.

Enterprise Server

server.enterprise.base

Use this license to start and run an Enterprise Server.

Enterprise Server under Enterprise Central

server.ec.es

Use this license to attach Enterprise Servers to an Enterprise Central.

Field bus devices under Enterprise Server

server.device.es

Use this license to attach Field bus devices to an Enterprise Server.

Automation server under Enterprise Server

server.es.as

Use this license to attach an automation server to an Enterprise Server.

Change Control

server.esignature

Use this license to allow Change Control.

Webservices, EWS Cons

server.ws.ews.consume

Use this license to start and run Web Services, EWS Consume.

Webservices, EWS Cons, SRV

server.ws.ews.server

Use this license to start and run Web Services, EWS Consume.

Webservices, EWS Cons, SRV

server.ws.ews.history

Use this license to start and run Web Services, EWS Consume.

Webservices, Generic Cons

server.ws.generic.consume

Use this license to start and run Web Services.

Cloud Connectivity

server.cloud.demo

Use this license to allow the server to connect to the cloud using Cloud Connectivity.

Sign PDF

server.dig.signed.docs

Use this license to get PDF reports digitally signed. One license is required for every Enterprise Central and Enterprise Server that uses the Sign PDF function.

  • Automation Server Licensing Overview