earth_america
user_standard Iniciar sessão
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interface de utilizador

Interface de utilizador


Produtos: SmartX Sensor
Funcionalidades: 3 botões, Hardware
Versão do produto: 3.3, 2022, 2023, 2024
22-07-2021

SpaceLogic Sensor 3-Button Cover Model Interface

Use the SpaceLogic Sensor 3-Button Cover model interface to change the temperature setpoint to a comfortable level. You can also confirm your presence in a room and turn on the lights with the occupancy override button.

 
action_zoom_plus_stroke SpaceLogic Sensor 3-Button Cover model interface
Imagem: SpaceLogic Sensor 3-Button Cover model interface

Tabela: SpaceLogic Sensor 3-Button Cover Model Interface

Button

Description

 
action_zoom_plus_stroke

Press to increase the temperature.

 
action_zoom_plus_stroke

Press to override current occupancy settings.

 
action_zoom_plus_stroke

Press to decrease the temperature.

  • SpaceLogic Sensor 3-Button Cover Model
  • Changing the Temperature Setpoint
  • Overriding the Occupancy Setting