earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: SpaceLogic Sensors
Functionalities: Hardware, Touchscreen
Product version: 3.3, 2022, 2023, 2024, 7.0, 7.1
7/23/2021

SpaceLogic Sensor Touchscreen Display Model- Front Menu Screen

Use the SpaceLogic Sensor Touchscreen Display model front menu screen to view and change the current settings and advance to the functions menu screen.

 
action_zoom_plus_stroke SpaceLogic Sensor Touchscreen Display model - front menu screen
Figure: SpaceLogic Sensor Touchscreen Display model - front menu screen

Table: SpaceLogic Sensor Touchscreen Display Model- Front Menu Screen

Button

Description

 
action_zoom_plus_stroke

Click this button to access the functions menu screen. For more information, see SpaceLogic Sensor Touchscreen Display Model- Functions Menu Screen .

The Allow menu page property on the SpaceLogic Sensor Display object property controls access to all submenus including the Functions menu and any of its submenus. If this property is turned off, you cannot access the functions menu and its submenus.

 
action_zoom_plus_stroke

Click this button to adjust the temperature setpoint. For more information, see Changing the Temperature Setpoint .

 
action_zoom_plus_stroke

Click this button to turn the lights on and off. For more information, see Turning the Lights On and Off .

 
action_zoom_plus_stroke

Click this button to open and close the blinds. For more information, see Fully Opening and Closing the Blinds .

 
action_zoom_plus_stroke

Click this button to access the scenes menu. For more information, see Selecting the Scenes Menu .

 
action_zoom_plus_stroke

Indicates that ECO mode heating or cooling is in effect in the SpaceLogic Sensor Touchscreen Display Model.

 
action_zoom_plus_stroke

Specifies the relative humidity setting in the room in which the SpaceLogic Sensor is located.

 
action_zoom_plus_stroke

Specifies the CO2 setting in the room in which the SpaceLogic Sensor is located.

  • SpaceLogic Sensor Touchscreen Display Model
  • SpaceLogic Sensor Touchscreen Display Model- Setpoint Adjustment Submenu