earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: SpaceLogic Sensors
Functionalities: Hardware, Touchscreen
Product version: 3.3, 2022, 2023, 2024, 7.0
7/23/2021

SpaceLogic Sensor Touchscreen Display Model- Setpoint Adjustment Submenu

When allowed, you can use the SpaceLogic Sensor Touchscreen Display model setpoint adjustment submenu to increase or decrease temperature and enhance living space comfort.

 
action_zoom_plus_stroke SpaceLogic Sensor Touchscreen Display model- setpoint adjustment submenu
Figure: SpaceLogic Sensor Touchscreen Display model- setpoint adjustment submenu

Table: SpaceLogic Sensor Touchscreen Display Model- Setpoint Adjustment Submenu

Button

Description

 
action_zoom_plus_stroke

Click this button to return to the previous menu screen.

 
action_zoom_plus_stroke

Click to increase the temperature. Click once for each full degree Fahrenheit and one-half degree Celsius of additional heat you want.

 
action_zoom_plus_stroke

Click to decrease the temperature.

 
action_zoom_plus_stroke

Indicates that you are restricted from raising or lowering the setpoint beyond three button clicks. For more information, see Changing the Temperature Setpoint in a Restricted Display .

  • SpaceLogic Sensor Touchscreen Display Model
  • SpaceLogic Sensor Touchscreen Display Model- Functions Menu Screen
  • Changing the Temperature Setpoint in a Restricted Display