Produkty: Czujnik SmartX
Funkcje: Sprzęt, Ekran dotykowy
Wersja produktu: 3.3, 2022, 2023, 2024, 7.0
2021-07-23

SpaceLogic Sensor Touchscreen Display Model- Setpoint Adjustment Submenu

When allowed, you can use the SpaceLogic Sensor Touchscreen Display model setpoint adjustment submenu to increase or decrease temperature and enhance living space comfort.

 
action_zoom_plus_stroke SpaceLogic Sensor Touchscreen Display model- setpoint adjustment submenu
Rysunek: SpaceLogic Sensor Touchscreen Display model- setpoint adjustment submenu

Tabela: SpaceLogic Sensor Touchscreen Display Model- Setpoint Adjustment Submenu

Button

Description

 
action_zoom_plus_stroke

Click this button to return to the previous menu screen.

 
action_zoom_plus_stroke

Click to increase the temperature. Click once for each full degree Fahrenheit and one-half degree Celsius of additional heat you want.

 
action_zoom_plus_stroke

Click to decrease the temperature.

 
action_zoom_plus_stroke

Indicates that you are restricted from raising or lowering the setpoint beyond three button clicks. Więcej informacji zawiera Changing the Temperature Setpoint in a Restricted Display .

  • SpaceLogic Sensor Touchscreen Display Model
  • SpaceLogic Sensor Touchscreen Display Model- Functions Menu Screen
  • Changing the Temperature Setpoint in a Restricted Display