Use the SmartX Sensor Touchscreen Display model main menu to perform a variety of tasks including:
Viewing menus and submenus
Adjusting temperature and fan speed
Changing occupancy mode or overrides
Changing unit views
Icon |
Description |
![]() |
Click to return to the default or home screen. |
![]() |
Click to view submenus (whenever applicable). |
![]() |
Click to toggle between fan speeds. If the fan speed icon is inactive, a lock icon displays to indicate that the Allow fan speed changes property in the Display object is turned off. You are not allowed to make fan speed changes. |
![]() |
Click to toggle between occupied and unoccupied settings. Click to also override current occupancy settings. If the override is off and not currently allowed, a lock icon displays. If the feature is not supported by the application, the occupancy icon is greyed out. |
![]() |
Click to toggle between Fahrenheit and Celsius degree settings. If the temperature units icon is inactive, a lock icon displays to indicate that the Allow temperature unit changes property in the Display object is turned off. You are not allowed to make temperature unit changes. |
![]() |
Click to toggle between heating and cooling mode. If HVAC mode is off, a lock icon displays here. It indicates that the Display object HVAC mode property is turned off and changes are not allowed. |