earth_america
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Как

Как


Продукты: WebStation
Функции: Тренды
Версия продукта: 2024, 7.0
02.12.2024

Showing Trend Chart Series as a List

You show trend log series as a list when you want to compare all values at the same time.

Показать больше
action_close

A trend log list displays all values in the trend log in a list.

In the trend log list, you can perform the following tasks:

  • View all the values and their time stamp.

  • Add and edit records, for example if you knew that some records might be wrong or are missing.

  • Export values as an Excel file.

  • Export values as an xml file.

  • View meter log changes.

  • View events.

  • Change the settings.

 
action_zoom_plus_stroke A Trend log list in WebStation
Рисунок: A Trend log list in WebStation

To show trend chart series as a list
  1. In WebStation, in the System tree pane, select the trend chart you want to show as a list.

  2. On the Trend Chart toolbar, click the Show as list button

     
    action_zoom_plus_stroke
    .

  • Trend Log Lists in WebStation