Log on to rate and give feedback
12345Log on to rate
0
Poradnik
Produkty:
WebStation
Funkcje:
Trendy
Wersja produktu:
2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023
2021-07-20
Automatically Updating Values in a Trend Chart Series
You automatically update values in a trend chart series so that you always see the latest value.
Pokaż więcej
action_close
You can display the trend logs as trend log series in a trend chart in a number of ways. For example, you can change the color and weight of the trend log line, or display markers at the time where the trend log value was sampled.
These settings can be saved so that the trend chart is displayed in the same way anytime you open it.
To automatically update values in a trend chart series
In WebStation, in the
System tree
pane, select the trend chart you want to automatically update.