Use the Schedule Settings dialog box to edit the configuration settings for the selected schedule.
Component |
Description |
Remove past events |
Select True to remove events that have already occurred from the selected schedule. |
Lead object |
Click to select a lead schedule if you want the selected schedule to be a shadow schedule. Więcej informacji zawiera Lead and Shadow Relationship . |
Default value |
Enter a default value for the selected schedule. |
Description |
Type a description for the selected schedule. |