earth_america
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Концепт

Концепт


Продукты: Контроллеры eCommission SmartX, IP-IO , MP-C, MP-V, RP-C, RP-V
Функции: Разработка, Контроллеры SmartX IP
Версия продукта: 2023, 2024, 7.0
17.12.2022

Connection Workflow for the Commission Mobile Application

Use this workflow to connect the Commission mobile application to BACnet/IP controllers.

Related information can be found in the sections that follow the flowchart.

 
action_zoom_plus_stroke Commission mobile application connection workflow
Рисунок: Commission mobile application connection workflow
Download, install, and log on to the Commission mobile application

Download, install, and log on to the Commission mobile application, and then accept the Terms of use agreement.

Более подробную информацию см. Logging on to the Commission Mobile Application .

Power up the controllers

Power up the BACnet/IP controllers.

Более подробную информацию см. Powering Up MP-C .

Более подробную информацию см. Powering Up MP-V .

Более подробную информацию см. Powering Up an RP-V Controller .

Prepare a wired or wireless connection for Commission mobile application

Prepare a wired or wireless connection for use with the Commission mobile application mobile device.

Connection Type

More Information

Wired connection to a single controller

Более подробную информацию см. Connecting to Single BACnet/IP Controller by Wire .

Wired connection to a network of controllers

Более подробную информацию см. Connecting to Network of BACnet/IP Controllers by Wire .

Wireless connection to a network of controllers via a WiFi router

Более подробную информацию см. Connecting to Network of BACnet/IP Controllers through WiFi Router .

Wireless connection to a network of controllers via a wireless access point

Более подробную информацию см. Connecting to Network of BACnet/IP Controllers through a Wireless Access Point .

Start the Commission mobile application and discover controllers

Start the Commission mobile application and then discover the BACnet/IP controllers on the network.

Более подробную информацию см. Logging on to the Commission Mobile Application .

  • Connection and Architecture Options
  • Logging on to the Commission Mobile Application
  • Powering Up MP-C
  • Powering Up MP-V
  • Powering Up an RP-V Controller
  • Connecting to Single BACnet/IP Controller by Wire
  • Connecting to Network of BACnet/IP Controllers by Wire
  • Connecting to Network of BACnet/IP Controllers through WiFi Router
  • Connecting to Network of BACnet/IP Controllers through a Wireless Access Point
  • Downloading and Starting the eCommission SmartX Controllers Mobile Application