earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Commission, IP-IO , MP-C, MP-V, RP-C
Functionalities: Engineering, BACnet/IP devices
Product version: 2022, 2023, 2024, 7.0
12/17/2021

Device Restart

Use the Device Restart function of the Commission mobile application to perform a restart of the BACnet/IP controller. There are four different ways to restart the BACnet/IP controller.

Restart Type

Description

Warm Start

Perform a Warm Start when you want to reset the controller and want to retain all Warm Start properties and Cold Start properties. Perform a Warm Start to troubleshoot any device malfunctions.

Cold Start

Perform a Cold Start when you want to reset the controller and want to retain all Cold Start properties which excludes Warm Start properties. Perform a Cold Start to troubleshoot any device malfunctions after a Warm Start has not resolved the issue.

Erase Controller Database

Erase the controller database to clear any applications in the controller and before deploying a new application. Erasing the controller database will retain only the network settings, RSTP, and BACnet ID. As a best practice, erase the controller database before deploying a new application to the controller.

For more information, see Restarting a BACnet/IP Controller .

  • Restarting a BACnet/IP Controller
  • Configuring BACnet/IP Device Settings