You can use the Controller List Creator function of the eCommission SmartX Controllers mobile application to capture device information from the Digital Matrix symbol on the tear-off product info labels of SmarX IP Controller devices.
The Controller List Creator saves this information in the background to a data file that can be exported as a comma-separated file for use in documenting the controllers at the job site.
In the Connection view, select the Controller List Creator button
In the Create Project dialog box, type a name in the Project name box.
Select Create . A controller data file is created in the background.
Select the Scan icon
If this is the first time the camera of the mobile device is used with the eCommission application, you may need to provide camera access to the eCommission application from the settings section of your mobile device or Windows 10 laptop.
Aim the camera at the Data Matrix symbol.
When the image capture succeeds, the List Creator view is displayed, and the Model , Serial number , and Ethernet MAC boxes are populated with data.
Type a description for the following fields:
In the Location box, type the location of the SmartX Controller device.
In the Equipment box, type a short description of the equipment that is associated with the SmartX Controller device.
In the Comment box, type a comment that you want to associate with the SmartX Controller device.
Continue capturing data from additional SmartX Controller devices as needed.
When you have captured all the controllers, select the File Management button
In the Project List view, select a project from the list.
In the Project List view, you can also review the list of existing projects and delete a project or create a new one.
For more information, see Managing Projects in the Controller List Creator .
Select the Export button
In the Export dialog box, copy the file path where the controller list file is located. To do this, select the path in the Location text box, choose Select All , and then select Copy to copy the text to the clipboard.
Select OK to export the data to a controller list file.
In the Project List view, select Continue .
Find the controller list file by navigating to the CommissioningTool\QR Code Report folder, using either of two methods:
File organization, and navigation within the file structure, varies from one Android platform to another. Therefore, you may need to try more than one approach when searching for the controller list file.
You can use a file navigation utility on the mobile device, for example File Explorer, to perform a search for the folder name.
You can follow the path you previously saved to the clipboard. To do this, start a file navigation utility on the mobile device, for example File Explorer, paste the path text into the search box, and then execute the search.
You have created a controller list file, which can be used to document the SmartX IP Controller devices within the system.