earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: User Management
Product version: 2024, 7.0
12/2/2024

Type Permissions

arrow1_rotationCustom Type Permissions arrow1_rotationIn-built Type Permissions arrow1_rotationType Permission Rules

Extended permissions for a type enable you to provide additional permissions for a particular user or groups of users by granting a specific set of permissions to a user accounts group or to a user account to all instances of this type. The purpose of extended type permissions is to increase the permissions for a specific type. There are two types of type permissions. Custom type permissions grant permissions for types created by the users. In-build type permissions grant permissions for types provided by default with the system.

Custom Type Permissions

Custom type permissions are type permissions for a type created by a user.

In-built Type Permissions

In-built type permissions are type permissions for a type provided by default with the system.

Type Permission Rules

You set permissions on a type twice.

First, you set permissions on the type of object. Types can be granted the following path permissions: Read, Write, Create, Delete, Edit, Force, Command and Inherited. You need to assign at least Read permissions on the type.

Second, you set permissions for user accounts and user account groups. A user account or a user account group can be granted or refused permissions to the type.

For more information, see Type Permissions Rules .

  • Extended Software Permissions
  • Type Permissions Rules