earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: User Management
Product version: 2023, 2024
12/17/2022

Assigning Type Permissions to User Accounts or User Account Groups

You assign type permissions to grant user accounts or user account groups access to a specific type in the EcoStruxure Building Operation software.

Show More
action_close

Extended permissions for a type enable you to provide additional permissions for a particular user or groups of users by granting a specific set of permissions to a user accounts group or to a user account to all instances of this type. The purpose of extended type permissions is to increase the permissions for a specific type. There are two types of type permissions. Custom type permissions grant permissions for types created by the users. In-build type permissions grant permissions for types provided by default with the system.

Custom Type Permissions

Custom type permissions are type permissions for a type created by a user.

In-built Type Permissions

In-built type permissions are type permissions for a type provided by default with the system.

Type Permission Rules

You set permissions on a type twice.

First, you set permissions on the type of object. Types can be granted the following path permissions: Read, Write, Create, Delete, Edit, Force, Command and Inherited. You need to assign at least Read permissions on the type.

Second, you set permissions for user accounts and user account groups. A user account or a user account group can be granted or refused permissions to the type.

For more information, see Type Permissions Rules .

To assign type permissions to user accounts or user account groups
  1. In WorkStation, in the System Tree pane, select the EcoStruxure BMS server you want to configure.

  2. Click the Control Panel tab.

  3. Click Account management .

  4. In the User Accounts list box or the User Account Groups list box, select the user account or the user account group, you want to assign the type permission to.

  5. Click Software permissions .

  6. In the Type Permissions pane, click +.

  7. Browse to the type you want to assign permissions to and click Select .

  8. Click the Save button

     
    action_zoom_plus_stroke
    .

    Note:

    You need at least Read permission on the path where the instance of the type belongs to.

Type permissions are assign to the user account or the user account group.

  • Type Permissions
  • Creating Type Permissions Templates