earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
1
如何

如何


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 用户管理
产品版本: 2023
2022/12/17

Creating Relative Path Templates

You create a relative path template to facilitate the process of assigning path permissions.

To create a relative path template
  1. In WorkStation, in the System Tree pane, select the EcoStruxure BMS server you want to configure.

  2. Click the Control Panel tab.

  3. Click Relative path permissions .

  4. In the File menu, click New and then click Relative path permissions .

  5. In the Create Object dialog box, in the Name box, type the name of your path permission.

  6. In the Path box, enter the path.

  7. In the Description box, type a description.

  8. Click Create .

  9. In the System Tree pane, select the relative path permission you just created.

  10. In the  Relative to box, browse to the path you want your permission to be relative to.

  11. Select + .

  12. In the Select Object window, select the object you want to add to the permission path.

  13. In the rules table, choose the permission level for the path.

  14. Click the Save button

     
    action_zoom_plus_stroke
    .

You can assign the created type permissions to user accounts or user account groups.