earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: User Management
Product version: 2023
5/13/2025

Assigning Relative Path Permissions to User Accounts or User Account Groups

You assign relative path permissions to grant user accounts or user account groups access to a specific path structure in the EcoStruxure Building Operation software.

Show More
action_close

Relative path permissions for a folder structure grant a specific set of permissions to a user account group or to a user account to all the folders accessible in a predefined path and its folder structure. Relative path permissions enable a user accounts group or a user account to reuse a specific path permission.

Furthermore, you can add and delete permissions for this folder structure.

Example

The same set of objects and properties (values, trends, alarms, graphics etc.) is defined in 100 rooms in your building. You define a relative path template that models the folder structure of the rooms in the building, and you define permissions to this folder structure. You define a relative path template by choosing one example of the folder structure. All similar folder structures following the same pattern will inherit permissions defined on the template. Finally, you also define permissions for specific user accounts and user account groups.

Relative Path Permissions Rules

You set permissions on a relative path twice.

First, you set permissions on the objects in the template. Objects in the template can be granted the following path permissions: Read, Write, Create, Delete, Edit, Force and Command.

Second, you set permissions for user accounts and user account groups. A user account or a user account group can be granted the following path permissions: Read, Write, Create, Delete, Edit, Force and Command.

For more information, see Relative Path Permissions Rules .

To assign a relative path permissions to user accounts or user account groups
  1. In WorkStation, in the System Tree pane, select the EcoStruxure BMS server you want to configure.

  2. Click the Control Panel tab.

  3. Click Account management.

  4. In the User Accounts list or the User Account Groups list, select the user account or the user account group, you want to assign the relative path permission to.

  5. Click Software permissions.

  6. In the Path Permissions pane, browse to the path you want and click +.

  7. In the permissions column, select permissions that you want to assign.

  8. In the Relative path permissions column, browse to the relative path permissions you want to use.

  9. Click the Save button

     
    action_zoom_plus_stroke
    .

You can edit and remove relative path permissions from user accounts and user account groups.

  • Relative Path Permissions
  • Editing Relative Path Permissions Templates
  • Creating Relative Path Templates