earth_america
user_standard Iniciar sesión
action_search_stroke
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
1
Explicación de procesos

Explicación de procesos


Productos AS-L, AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Gestión de usuarios
Versión del producto: 2.0, 2.1, 3.0, 3.1
04/09/2018

Editing Relative Path Permissions Templates

You modify a relative path permission by adding or withdrawing permissions for this folder structure. The changes will be accounted in all the instance.

To edit a relative path permissions template
  1. In Workstation, in the System Tree pane, select the EcoStruxure BMS server you want to configure.

  2. Click the Control Panel tab.

  3. Click Relative path permissions .

  4. In the Tree Pane select the relative path permissions you want to edit.

  5. In the permissions column, select permissions that you want to assign and unselect permissions you want to withdraw.

  6. Click the Save button

     
    action_zoom_plus_stroke
    .

You modified permissions that user accounts and user account groups have to a folder structure.