Produits : AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Fonctionnalités : Gestion des utilisateurs
Version produit : 2024, 7.0
02/12/2024

Removing Relative Path Permissions from User Accounts or User Account Groups

You remove relative path permissions from user accounts or user account groups to modify users access to spacific folder structures.

Afficher plus
action_close

You set permissions on a relative path twice.

First, you set permissions on the objects in the template. Objects in the template can be granted the following path permissions: Read, Write, Create, Delete, Edit, Force and Command.

Second, you set permissions for user accounts and user account groups. A user account or a user account group can be granted the following path permissions: Read, Write, Create, Delete, Edit, Force and Command.

Table : Software Permissions Rules

Property

Description

Read

Permits viewing and listing path content

Write

Permits an administrator to change configurations except for bindings, programs, and graphics

Create

Permits creating new objects on the path

Delete

Permits deleting objects under the path. Delete permissions are required on a folder to delete its contents

Edit

Permits editing objects on the path

Force

Permits forcing values on the path

Command

Permits the execution of commands on the path. Command permissions can override this permission for specific commands

Inherited

Indicates that the permissions are inherited from the parent folder

Déclaration

You need delete permissions to rename, paste and duplicate folders and objects in EcoStruxure Building Operation software.

Déclaration

You can always edit graphic and program objects in the relevant editor, however in order to save it on your server you need "Edit" permissions. You can save your edits on your hard drive or export to a location of your choice even if you don’t have “Edit” permissions.

To remove relative path permissions from user accounts or user account groups
  1. In WorkStation, in the System Tree pane, select the EcoStruxure BMS server you want to configure.

  2. Click the Control Panel tab.

  3. Click Account management .

  4. In the User Accounts list box or the User Account Groups list box, select the user account or the user account group you want to remove the relative path permissions from.

  5. Click Software permissions .

  6. In the Path Permissions pane, browse to the path you want to remove.

  7. In the Relative path permissions column erase the url.

  8. Click the Save button

     
    action_zoom_plus_stroke

User accounts or user account groups are no longer granted permissions to a specific folder structure.

  • Relative Path Permissions Rules
  • Software Permissions Rules Management
  • Software Permissions, User Accounts, and User Account Groups
  • User Account – Software Permissions Tab
  • User Account Group – Software Permissions Tab
  • Creating Relative Path Templates
  • Editing Relative Path Permissions Templates
  • Deleting Relative Path Templates
  • Assigning Relative Path Permissions to User Accounts or User Account Groups