earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: AS-B, Enterprise Server, ​License Administrator, ​License Server, AS-P, Virtual Project Servers
Functionalities: License Management
Product version: 3.2
3/19/2021

License Information Enterprise Server

Use License Information to check the licenses for an Enterprise Server and the attached SmartX servers.

 
action_zoom_plus_stroke License Information
Figure: License Information

Table: License Information

Property

Description

SmartX servers

Displays the number of licenses for SmartX Servers attached to the EcoStruxure BMS server. For more information, see License Information .

Fieldbus Device

Displays the number of licenses for the fieldbus devices attached to the Enterprise Server. For more information, see License Information .

SmartDrivers

Displays the number of licenses for the Smart driver devices attached to the EcoStruxure BMS server and SmartX AS-P server. For more information, see License Information .

SNMP Notification

Display the licenses for the SNMP notification for each EcoStruxure BMS server. SNMP notification required one license per server. For more information, see License Information .

Change Control

Display the licenses for Change Control for each EcoStruxure BMS server. Change Control required one license per server. For more information, see License Information .

TimescaleDB

Display the licenses for TimescaleDB for each EcoStruxure BMS server. For more information, see License Information .

PDF Sign ing

Display the Sign PDF licenses. One license is required for every Enterprise Central and Enterprise Server that uses the Sign PDF function. For more information, see License Information .

MQTT Read/Write

Display the license for an MQTT client, on an Enterprise Server or SmartX server, to read and write to an MQTT broker. A valid license on an Enterprise Server are inherited by all attached SmartX servers. For more information, see License Information .

Subserver

Displays the license status for the attached SmartX servers. For more information, see License Information .

  • License Information
  • License Information Enterprise Central