earth_america
user_standard Logga in
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Koncept

Koncept


Produkter: SmartX Sensor
Funktionaliteter: 3-knappars, Maskinvara, LCD, Pekskärm
Produktversion: 3.3, 2022, 2023, 2024, 7.0
2021-07-23

SpaceLogic Sensor Models

SpaceLogic Sensor include blank cover and occupancy sensor-only cover models, as well as several models with pushbutton or display-driven user interfaces that allow you to control temperature, occupancy, overrides, and a variety of other settings in a designated living space.

 
action_zoom_plus_stroke SpaceLogic Sensor models
Figur: SpaceLogic Sensor models

SpaceLogic Sensor 3-button Cover Model

The 3-Button Cover model contains a passive, infrared sensor for occupancy detection and a plus and minus button to adjust the temperature setpoint. There is also an occupancy override button should the room occupant wish to confirm their presence, turn on the lights, and change the setpoint to a comfortable level.

Mer information finns i SpaceLogic Sensor 3-Button Cover Model .

SpaceLogic Sensor LCD Temperature Sensor Model

The LCD Temperature Sensor model is the relatively inexpensive, mid-range model with a small LCD display and three buttons to increment (plus), decrement (minus) and then select options (middle button) as you scroll through its menus.

Mer information finns i SpaceLogic Sensor LCD Temperature Sensor Model .

SpaceLogic Sensor Touchscreen Display Model

The Touchscreen Display model provides a menu-driven interface with a main menu and an optional default or home screen configurable through EcoStruxure Building Operation.

Mer information finns i SpaceLogic Sensor Touchscreen Display Model .

  • SpaceLogic Sensor Modular Bases and Covers
  • SpaceLogic Sensor 3-Button Cover Model Interface
  • SpaceLogic Sensor LCD Temperature Sensor Model
  • SpaceLogic Sensor Touchscreen Display Model