earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: SmartX Sensor
功能: 3 个按钮, 硬件, LCD, 触摸屏
产品版本: 3.3, 2022, 2023, 2024, 7.0
2021/7/23

SpaceLogic Sensor Models

SpaceLogic Sensor include blank cover and occupancy sensor-only cover models, as well as several models with pushbutton or display-driven user interfaces that allow you to control temperature, occupancy, overrides, and a variety of other settings in a designated living space.

 
action_zoom_plus_stroke SpaceLogic Sensor models
图: SpaceLogic Sensor models

SpaceLogic Sensor 3-button Cover Model

The 3-Button Cover model contains a passive, infrared sensor for occupancy detection and a plus and minus button to adjust the temperature setpoint. There is also an occupancy override button should the room occupant wish to confirm their presence, turn on the lights, and change the setpoint to a comfortable level.

有关更多信息,请参阅 SpaceLogic Sensor 3-Button Cover Model .

SpaceLogic Sensor LCD Temperature Sensor Model

The LCD Temperature Sensor model is the relatively inexpensive, mid-range model with a small LCD display and three buttons to increment (plus), decrement (minus) and then select options (middle button) as you scroll through its menus.

有关更多信息,请参阅 SpaceLogic Sensor LCD Temperature Sensor Model .

SpaceLogic Sensor Touchscreen Display Model

The Touchscreen Display model provides a menu-driven interface with a main menu and an optional default or home screen configurable through EcoStruxure Building Operation.

有关更多信息,请参阅 SpaceLogic Sensor Touchscreen Display Model .

  • SpaceLogic Sensor Modular Bases and Covers
  • SpaceLogic Sensor 3-Button Cover Model Interface
  • SpaceLogic Sensor LCD Temperature Sensor Model
  • SpaceLogic Sensor Touchscreen Display Model