earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: SmartX Sensor
功能: 3 个按钮, 硬件, LCD, 触摸屏
产品版本: 3.1, 3.2
2019/12/19

SmartX Sensor Models

SmartX Sensors include blank cover and occupancy sensor-only cover models, as well as several models with pushbutton or display-driven user interfaces that allow you to control temperature, occupancy, overrides, and a variety of other settings in a designated living space.

 
action_zoom_plus_stroke SmartX Sensor models
图: SmartX Sensor models

SmartX Sensor 3-button Cover Model

The 3-Button Cover model contains a passive, infrared sensor for occupancy detection and a plus and minus button to adjust the temperature setpoint. There is also an occupancy override button should the room occupant wish to confirm their presence, turn on the lights, and change the setpoint to a comfortable level.

有关更多信息,请参阅 SmartX Sensor 3-Button Cover Model .

SmartX Sensor LCD Temperature Sensor Model

The LCD Temperature Sensor model is the relatively inexpensive, mid-range model with a small LCD display and three buttons to increment (plus), decrement (minus) and then select options (middle button) as you scroll through its menus.

有关更多信息,请参阅 SmartX Sensor LCD Temperature Sensor Model .

SmartX Sensor Touchscreen Display Model

The Touchscreen Display model provides a menu-driven interface with a main menu and an optional default or home screen configurable through EcoStruxure Building Operation.

有关更多信息,请参阅 SmartX Sensor Touchscreen Display Model .

  • SmartX Sensor Modular Bases and Covers
  • SmartX Sensor 3-Button Cover Model Interface
  • SmartX Sensor LCD Temperature Sensor Model
  • SmartX Sensor Touchscreen Display Model