earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Commission, MP-C, MP-V, SpaceLogic Sensors
Functionalities: Hardware
Product version: 3.0, 3.1
8/28/2019

eCommission Bluetooth Adapter

arrow1_rotationSpecifications

The eCommission Bluetooth Adapter is plugged into a SmartX Sensor to provide a wireless Bluetooth connection to the SmartX IP controller (Sensor Bus compliant controller) for commissioning, maintenance, and troubleshooting of the controller and the sensor.

Notice

SMARTX SENSOR OR OTHER EQUIPMENT DAMAGE

  • Plug in the adapter with the button to the front.

  • Do not plug into any device other than a SmartX Sensor.

Failure to follow these instructions can result in equipment damage.

 
action_zoom_plus_stroke  eCommission Bluetooth Adapter provides Bluetooth access to SmartX IP controllers
Figure: eCommission Bluetooth Adapter provides Bluetooth access to SmartX IP controllers

The eCommission Bluetooth Adapter provides a bridge between a Bluetooth enabled mobile device running the eCommission SmartX Controllers mobile application and the Sensor Bus on the SmartX IP controller. The eCommission mobile application is used to perform commissioning, flow balance, and checkout operations on SmartX IP controllers. For more information, see eCommission SmartX Controllers Mobile Application Overview .

The Bluetooth adapter is designed to be connected to a SmartX Sensor, which in turn is connected to the Sensor Bus port on the SmartX IP controller. The Bluetooth adapter cannot be connected directly to the Sensor Bus port on the SmartX IP controller. For more information, see SmartX IP Controller Sensor Bus .

The Bluetooth adapter is plugged into a connector on the upper-right side of the SmartX Sensor. For more information, see Installing eCommission Bluetooth Adapter on a SmartX Sensor . The physical connector on the sensor is a USB style connector, but the electrical interface and communication protocol are not USB. The Bluetooth adapter communicates with the SmartX IP controller over the Sensor Bus using the RS-485 physical layer.

The Bluetooth adapter PCB has a card-edge connector that protrudes from the PCB and mates with the SmartX Sensor connector.

The Bluetooth adapter is powered by the SmartX Sensor, which also provides transient protection to the adapter.

The Bluetooth adapter is housed in a plastic enclosure, which has a protective cap to help protect the PCB card edge when the adapter is not connected to a SmartX Sensor. The protective cap has a hinge mechanism. The cap can either hang down, or rotate to the back end and snap on, when the adapter is connected to a SmartX Sensor. The adapter is delivered with a lanyard that can be attached to a loop on the protective cap. For more information, see Attaching a Lanyard to eCommission Bluetooth Adapter .

 
action_zoom_plus_stroke eCommission Bluetooth Adapter
Figure: eCommission Bluetooth Adapter

The Bluetooth adapter has a momentary push-button switch that is used for pairing the adapter with a mobile device running the eCommission SmartX Controllers mobile application. For more information, see Connecting to a Controller with the Bluetooth Adapter .The Bluetooth adapter sends out a unique signal that enables the mobile device to pair with the correct adapter. A blue indicator LED on the adapter indicates the status.

Table: eCommission Bluetooth Adapter LED Patterns

LED Patterns

Condition/Mode

Blue, flashing (2 s ON, 8 s OFF)

Default Mode (No Bluetooth client connection, no SmartX IP controller connection)

Blue, flashing (1 s ON, 1 s OFF)

Advertising Mode (No Bluetooth client connection, no SmartX IP controller connection, connection is possible)

Blue, constant (always ON)

Connected Mode (Bluetooth client connection, no SmartX IP controller connection)

Blue, ON when transmitting, OFF otherwise

Active Mode (Bluetooth client connection, SmartX IP controller connection active)

Blue, flashing (2 s ON, 6 s OFF, 8 s ON, 4 s OFF)

DFU Mode (Waiting for user to press and hold push-button)

Specifications

Electrical
DC input power consumption
Maximum 0.25 W
DC input supply voltage
5.0 to 5.5 VDC (powered by the SmartX Sensor)
Communications
Wireless communications
Bluetooth ® 4.2 Low Energy compliant
  
Bluetooth ® 5 Advertising
  
Frequency: 2.4 GHz
  
Line-of-sight range: max. 50 m (164 ft)
SmartX communications
RS-485, proprietary Sensor Bus protocol
Operation environment
Ambient temperature, operating
0 to 50 °C (32 to 122 °F)
Ambient temperature, storage
-40 to +70 °C (-40 to +158 °F)
Humidity
Maximum 95 % RH non-condensing
Mechanical
Dimensions
70 W x 32 H x 12 D mm (2.8 W x 1.3 H x 0.5 D in.)
Weight
0.02 kg (0.05 lb) with lanyard
Hardware
CPU type
ARM Cortex-M4 single-core
Frequency
38.4 MHz
SRAM (embedded)
32 KB
Flash memory (embedded)
256 KB
Flash memory (serial)
1 MB
Status indicator
LED (blue)
Button
Momentary push-button switch
  • Hardware Overview
  • eCommission SmartX Controllers Mobile Application Overview
  • SmartX IP Controller Sensor Bus
  • Installing eCommission Bluetooth Adapter on a SmartX Sensor
  • Attaching a Lanyard to eCommission Bluetooth Adapter
  • Connecting to a Controller with the Bluetooth Adapter