earth_america
user_standard Zaloguj się
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Pojęcie

Pojęcie


Produkty: WebStation
Funkcje: Dashboards
Wersja produktu: 3.0, 3.1, 3.2, 3.3, 2022, 2023
2024-02-23

Heat Map

A heat map is a graphical representation of data where the values contained in a matrix are represented as colors.

Heat map is typically used to present a trend log. A Heat map can be used to display any information, for example temperature, water consumption, or energy consumption.

The color and scale of the blocks in the Heat map can be changed to fit its content. For example, cooling can be displayed in various blue shades and heating in various yellow and red shades.

  • How Dashboards Work
  • Dashboard Widgets
  • Configuring a Heat Map