earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: RP-C
功能: 硬件
产品版本: 3.1
2019/12/19

RP-C Communication Ports

The RP-C contains a combination of Ethernet, USB, SmartX Sensor, and Connected Room Solution communication ports.

This combination includes the following ports:

  • Two 10/100 Ethernet ports

  • One USB host port

  • One USB device port

  • One Sensor bus port

  • One Room bus port

When both Ethernet ports are enabled, they function as an onboard Ethernet switch. Disabling the second Ethernet port disables the switching function. The switching function enables flexible network topologies. 有关更多信息,请参阅 SmartX IP Controller Network Topologies . The second port also provides a connection point for a laptop running the eCommission SmartX Controllers mobile application.

The two USB ports are reserved for future use.

The Sensor bus port is designed for connection of SmartX Sensors. 有关更多信息,请参阅 SmartX IP Controller Sensor Bus .

The Room bus port is designed for connection of RP Series expansion modules and multi-sensors for connected room solutions. 有关更多信息,请参阅 RP-C Room Bus .

  • Hardware Overview
  • RP-Cs
  • SmartX IP Controller Network Topologies
  • SmartX IP Controller Sensor Bus
  • RP-C Room Bus