The RP-C has fixed screw terminals for the power input, SSR outputs, relay outputs, high power relay outputs, and universal inputs/outputs.
The wiring recommendations are provided separately. 有关更多信息,请参阅 Wiring .
The RP-C-12A model has 12 I/O points and the controller is equipped with 23 fixed screw terminals.
有关更多信息,请参阅 RP-C-12A Screw Terminals .
The RP-C-12B model has 12 I/O points and the controller is equipped with 24 fixed screw terminals.
有关更多信息,请参阅 RP-C-12B Screw Terminals .
The RP-C-12C model has 12 I/O points and the controller is equipped with 24 fixed screw terminals.
有关更多信息,请参阅 RP-C-12C Screw Terminals .
The RP-C-16A model has 16 I/O points and the controller is equipped with 30 fixed screw terminals.
有关更多信息,请参阅 RP-C-16A Screw Terminals .