earth_america
user_standard Zaloguj się
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Pojęcie

Pojęcie


Produkty: RP-C
Funkcje: Sprzęt
Wersja produktu: 2022
2023-12-12

RP-C LEDs

arrow1_rotationStatus LED

There is one LED on the front panel of the RP-C.

 
action_zoom_plus_stroke RP-C LEDs
Rysunek: RP-C LEDs

Tabela: RP-C LEDs

Function

Color

Status

Red, Green, Blue (and combinations)

Status LED

The RP controller Status LED indicates the condition of the device.

Tabela: RP Controller Status LED Patterns

LED Patterns

Condition

Green, constant

Normal operation, status OK

RP controller firmware application running

No Bluetooth activity

Blue, constant

Normal operation, status OK

RP controller firmware application running

Bluetooth connection is active

Green 3 seconds, blue 1 second

Normal operation, status OK

RP controller firmware application running

Bluetooth advertising is active

Green, flashing (~1 Hz)

Device restarting, wait

RP controller firmware application running

Red, constant

Detected error, attention required

Red, flashing (~1 Hz)

Device operates, but a problem needs attention

Red/blue, flashing (~1 Hz) a

Bluetooth radio microcontroller firmware is being upgraded

Red/green, flashing (~1 Hz)

RP I/O board receiving software upgrade, wait

Do not interrupt power to the controller. For more information, see the following Important note.

Amber, constant

RP controller firmware boot applet running

Amber, flash

Device restarting, wait

RP controller firmware boot applet started

Amber/green, flashing (~1 Hz)

RP controller firmware is being upgraded. It is typically the firmware main application, but it can also be a boot applet.

White, transient

Device starting, wait

White, constant

RP controller firmware not running, attention required (contact product support)

Uwaga

Avoid power interruptions to the device during the brief period when the Status LED is flashing red and green. An interruption causes problems with the I/O processor upgrade and can result in corrupt firmware. You can view the evidence of a corrupt processor when the device reports itself as an “MP-C-15A.” A corrupt I/O processor can lead to the loss of the reset button and/or I/O functionality, as well as the inability to upgrade the I/O processor and/or the device.

  • RP-C Controllers
  • Status LEDs