earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: WebStation
Functionalities: Dashboards
Product version: 3.0, 3.1, 3.2, 3.3, 2022, 2023
2/23/2024

Heat Map Properties Dialog Box

Use the Heat Map Properties dialog box to configure and edit a heat map.

 
action_zoom_plus_stroke Heat map properties dialog box
Figure: Heat map properties dialog box

Table: Heat Map Properties Dialog Box

Component

Description

Display trend log

Enter the trend log you want to display.

Period

Select the period you want to display.

Calculation method

Select the calculation method for the trend log. For more information, see Calculation Methods .

Caption

Type a caption for the widget.

Caption Link

Select to make a link to an object that is relevant to the values that are displayed in the widget.

Show legend

Click True to display the name and color of the trend log in the widget.

Guides

Use the guides to define the colors for different values and value ranges.

For more information, see Heat Map .

Add

Click to add a guide to define the colors for different values and value ranges.

For more information, see Heat Map .

Value

Select a value for the guide in the widget.

Color

Select a color for the value for the guide in the widget.

Decimals

Select the number of decimals you want to display.

  • Dashboard Widgets
  • Heat Map
  • Widget Dialog Box – Layout Tab