earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: WebStation
功能: Dashboards
产品版本: 2024, 7.0
2024/12/2

Log Gauge Properties Dialog Box

Use the Log Gauge Properties dialog box to configure and edit a log gauge.

 
action_zoom_plus_stroke Log Gauge properties – dialog box
图: Log Gauge properties – dialog box

表格: Log Gauge Properties – Dialog Box

Component

Description

Display trend log

Enter the trend log you want to display.

Period

Select the period you want to display.

Calculation method

Select the calculation method for the trend log. 有关更多信息,请参阅 Calculation Methods .

Caption

Type a caption for the widget.

Caption Link

Select to make a link to an object that is relevant to the values that are displayed in the widget.

Min

Enter the minimum value for the gauge.

Max

Enter the maximum value for the gauge.

Guides

Use the guides to define the colors for different values and value ranges.

有关更多信息,请参阅 Log Gauge .

Add

Click to add a guide to define the colors for different values and value ranges.

有关更多信息,请参阅 Log Gauge .

Value

Select a value for the guide in the widget.

Color

Select a color for the value for the guide in the widget.

Description

Type a description.

Indicator color

Select the indicator color for the needle or the indicator in the gauge.

有关更多信息,请参阅 Log Gauge .

Decimals

Select the number of decimals you want to display.

Show Period

Select to display the period as a legend.

Use needle

Select True to use a needle as indicator in the gauge. If no needle is selected the gauge displays the value as an indicator instead.

  • 仪表板小部件
  • Log Gauge
  • Widget Dialog Box – Layout Tab