earth_america
user_standard Logga in
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Användargränssnitt

Användargränssnitt


Produkter: WebStation
Funktionaliteter: Dashboards
Produktversion: 3.0, 3.1, 3.2, 3.3, 2022, 2023
2024-02-23

Log Value Properties Dialog Box

Use the Log Value Properties dialog box to configure and edit a log value.

 
action_zoom_plus_stroke Log value properties dialog box
Figur: Log value properties dialog box

Tabell: Log Value Properties Dialog Box

Component

Description

Add

Click to add a trend log.

Display trend log

Enter the trend log you want to display.

Icon

Select an icon to be displayed in front of the value.

Calculation method

Select the calculation method for the trend log. Mer information finns i Calculation Methods .

Period

Select the period you want to display.

Caption

Type a caption for the widget.

Caption Link

Select to make a link to an object that is relevant to the values that are displayed in the widget.

Show Period

Select to display the period as a legend.

  • Dashboard Widgets
  • Log Value
  • Widget Dialog Box – Layout Tab