Use the Period over Period Chart Properties dialog box to configure and edit a period over period chart.
Component |
Description |
Add |
Click to add a trend log. |
Display trend log |
Enter the trend log you want to display. |
Chart type |
Select the type of chart you want to display. |
Calculation method |
Select the calculation method for the trend log. For more information, see Calculation Methods . |
Color |
Select the color you want to use for the trend log. |
Y-axis |
Select the position of the y-axis. |
Missing data |
Select how to display missing data. |
Period |
Select the period you want to display. |
Caption |
Type a caption for the widget. |
Caption Link |
Select to make a link to an object that is relevant to the values that are displayed in the widget. |
Show Legend |
Click True to display the name and color of the trend log in the widget. |
Show Period |
Select to display the period as a legend. |
Stack series |
Select to stack the series. |
Y-axis minimum |
Enter the Y-axis minimum. |
Y-axis maximum |
Enter the Y-axis maximum. |
Decimals |
Select the number of decimals you want to display. |