Produkty: WebStation
Funkcje: Dashboards
Wersja produktu: 3.0, 3.1, 3.2, 3.3, 2022, 2023
2024-02-23

XY Plot Properties Dialog Box

Use the XY Plot Properties dialog box to configure and edit a XY plot.

 
action_zoom_plus_stroke XY plot properties dialog box
Rysunek: XY plot properties dialog box

Tabela: XY Plot Properties Dialog Box

Component

Description

X-Axis Log

Enter log you want to display on the x-axis.

X-Axis Calculation method

Select the calculation method for the X-Axis.

Y-Axis Log

Enter the log you want to display on the y-axis.

Y-Axis Calculation method

Select the calculation method for the Y-axis.

Period

Select the period you want to display.

Calculated Period

Select the time span for which the calculation method is to be executed.

Scatter

Select to display all values as individual points in the diagram. Więcej informacji zawiera XY Plot .

Contour

Select to display a contour map of the correlation of values. Więcej informacji zawiera XY Plot .

Gridlines

Select to display gridlines in the diagram.

Linear Regression Line

Select to display a linear regression line. Więcej informacji zawiera XY Plot .

Polynomial Regression Curve

Select to display a polynomial regression line. Więcej informacji zawiera XY Plot .

Caption

Type a caption for the widget.

Caption Link

Select to make a link to an object that is relevant to the values that are displayed in the widget.

Show Period

Select to display the period as a legend.

X-Axis Caption

Enter a caption for the X-axis.

Y-Axis Caption

Enter a caption for the Y-axis.

Point Color

Select the color for the points in the diagram. Więcej informacji zawiera XY Plot .

Inner Contour Color

Select the inner color for a contour map in the diagram. Więcej informacji zawiera XY Plot .

Outer Contour Color

Select the outer color for a contour map in the diagram. Więcej informacji zawiera XY Plot .

Line Color

Select the color for a linear regression line in the diagram. Więcej informacji zawiera XY Plot .

X-Axis Minimum

Select the X-axis minimum.

X-Axis Maximum

Select the X-axis maximum.

Y-Axis Minimum

Select the Y-axis minimum.

Y-Axis Maximum

Select the Y-axis maximum.

Decimals

Select the number of decimals you want to display.

  • Dashboard Widgets
  • XY Plot
  • Widget Dialog Box – Layout Tab