earth_america
user_standard Logga in
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Användargränssnitt

Användargränssnitt


Produkter: WebStation
Funktionaliteter: Dashboards
Produktversion: 2024, 7.0
2024-12-02

XY Plot Properties Dialog Box

Use the XY Plot Properties dialog box to configure and edit a XY plot.

 
action_zoom_plus_stroke XY plot properties dialog box
Figur: XY plot properties dialog box

Tabell: XY Plot Properties Dialog Box

Component

Description

X-Axis Log

Enter log you want to display on the x-axis.

X-Axis Calculation method

Select the calculation method for the X-Axis.

Y-Axis Log

Enter the log you want to display on the y-axis.

Y-Axis Calculation method

Select the calculation method for the Y-axis.

Period

Select the period you want to display.

Calculated Period

Select the time span for which the calculation method is to be executed.

Scatter

Select to display all values as individual points in the diagram. Mer information finns i XY Plot .

Contour

Select to display a contour map of the correlation of values. Mer information finns i XY Plot .

Gridlines

Select to display gridlines in the diagram.

Linear Regression Line

Select to display a linear regression line. Mer information finns i XY Plot .

Polynomial Regression Curve

Select to display a polynomial regression line. Mer information finns i XY Plot .

Caption

Type a caption for the widget.

Caption Link

Select to make a link to an object that is relevant to the values that are displayed in the widget.

Show Period

Select to display the period as a legend.

X-Axis Caption

Enter a caption for the X-axis.

Y-Axis Caption

Enter a caption for the Y-axis.

Point Color

Select the color for the points in the diagram. Mer information finns i XY Plot .

Inner Contour Color

Select the inner color for a contour map in the diagram. Mer information finns i XY Plot .

Outer Contour Color

Select the outer color for a contour map in the diagram. Mer information finns i XY Plot .

Line Color

Select the color for a linear regression line in the diagram. Mer information finns i XY Plot .

X-Axis Minimum

Select the X-axis minimum.

X-Axis Maximum

Select the X-axis maximum.

Y-Axis Minimum

Select the Y-axis minimum.

Y-Axis Maximum

Select the Y-axis maximum.

Decimals

Select the number of decimals you want to display.

  • Dashboard Widgets
  • XY Plot
  • Widget Dialog Box – Layout Tab