earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: WebStation
功能: Dashboards
产品版本: 2024, 7.0
2024/12/2

Point Value Properties Dialog Box

Use the Point Value Properties dialog box configure and edit a point value.

 
action_zoom_plus_stroke Point value properties dialog box
图: Point value properties dialog box

表格: Point Value Properties Dialog Box

Component

Description

Add

Click to add a point.

Display variable

Enter the variable you want to display.

Icon

Select an icon to be displayed in front of the value.

Caption

Type a caption for the widget.

Caption Link

Select to make a link to an object that is relevant to the values that are displayed in the widget.

  • 仪表板小部件
  • Point Value
  • Widget Dialog Box – Layout Tab