earth_america
user_standard Zaloguj się
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Poradnik

Poradnik


Produkty: WebStation
Funkcje: Dashboards
Wersja produktu: 3.0, 3.1, 3.2, 3.3, 2022, 2023
2024-02-23

Configuring a Log Gauge

You configure a log gauge to display a trend log in a gauge.

Pokaż więcej
action_close

A log gauge displays trend log values in a gauge.

Using the guides, you can configure the scale of the gauge to display different colors in different ranges on the scale.

You can use two methods to display the value in the gauge a needle or an indication scale inside the gauge.

For example, you want a log gauge that displays log values between 0 and 30. Values under 10 are too low and will be marked blue. Values between 10 and 20 are ok and will be marked green. Values between 20 and 30 are too high and will be marked red. You want a needle to indicate the value on the gauge scale.

Configure the scale for the gauge using the min value 0 and the max value 30.

Add three Guides in the Guide field. Configure them as follows:

  • Value = 10 and color blue. This makes the value range 0 to 10 blue in the gauge.

  • Value = 20 and color green. This makes the value range 11 to 20 green in the gauge.

  • Value = 30 and color red. This makes the value range 21 to 30 red in the gauge.

You can make the indicator color black and use the needle to display the value.

If you set the indicator color to black but forget to set Use needle to true you get a black indicator inside the gauge that displays the value.

To configure a log gauge
  1. Click Configure or click the Settings button

     
    action_zoom_plus_stroke
    .

  2. In the Log Gauge Properties dialog box, in the Display trend log box, enter the trend log you want to display as a log gauge.

  3. In the Period box, select a period.

  4. In the Calculation method box, select a calculation method.

  5. In the Caption box, type a caption.

  6. In the Caption Link box, enter a link to an object that is relevant for the log gauge.

  7. In the Min box, enter the lowest value of the gauge.

  8. In the Max box, enter the highest value of the gauge.

  9. Click Add to add a guide to define the colors for different values and value ranges.

  10. In the Value box, enter a value for the guide.

  11. In the Color box, enter a color for the value or value range.

  12. In the Description box, enter a description for the guide.

  13. In the Indicator color box, enter the indicator color for the needle or the indicator in the gauge.

  14. In the Decimal box, select the number of decimals to dispaly.

  15. In the Show Period box, select True to display the period as a legend.

  16. In the Use needle box, select True to use a needle as indicator in the gauge. If no needle is selected the gauge displays the value as an indicator instead.

  17. Click OK .

  • How Dashboards Work
  • Dashboard Widgets
  • Log Gauge
  • Log Gauge Properties Dialog Box
  • Adding a Widget to a Dashboard