Use the Select Dashboard Widget s dialog box to add widgets, graphics, and hyperlinks to a dashboard.
Component |
Description |
Quick filter |
Enter a word or a character to filter on. For more information, see Quick Filter . |
Widgets |
Click on the widget you want to add to the dashboard. |
Browse |
Click to browse to add a hyperlink or a graphic to the dashboard. For more information, see Graphics in Dashboards . |
Graphics |
Click to add a custom type graphic to the dashboard. For more information, see Graphics in Dashboards . |