earth_america
user_standard Connexion
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Produits : AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Fonctionnalités : Fonctionnalité de base
Version produit : 2024, 7.0
02/12/2024

Show Abbreviated References

References in the List view are abbreviated to save space. An abbreviated reference might only display the first part of the reference but sometimes the last part is the most important one. You can have the system only show the last part of the reference in the list.

For example, if the full reference is ../../IO Resources/Onboard IO/DO 01 and you select to show abbreviated references, the list shows DO 01.

  • List View Toolbar
  • Basic Functions
  • Showing Abbreviated References