earth_america
user_standard Zaloguj się
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Poradnik

Poradnik


Produkty: WebStation
Funkcje: Dashboards
Wersja produktu: 3.0, 3.1, 3.2, 3.3, 2022, 2023
2024-02-23

Allowing a User to Access Personal Favorites

You allow the members of a group to access personal favorites so that they can create a personal overview of their system. The setting for this is done at the group level.

Pokaż więcej
action_close

Using WebStation, you can create and administer user accounts.

You can also add a new user account to an already existing user group in the system. You can force users to change their password the next time they log on. Unused accounts can be disabled and saved for further use or they can be deleted from the system.

To allowing a user to access Personal Favorites
  1. In WebStation, click System .

  2. In the System pane, click Domains .

  3. In the Domains pane, click Groups .

  4. Click the group.

  5. Select Allow members to access Personal Favorites .

  6. Click Save .

  • Create and Administer User Accounts in WebStation
  • Allowing a User to Access Personal Dashboards