You create a slideshow to automatically switch the display of different dashboards.
In WebStation, right-click the folder where you want to create the slideshow.
Click Create Slideshow .
In the Create object - slideshow dialog, in the Name box type a name for the slideshow.
Click OK .
Click Configure .
In the Speed(s) row, enter the interval between dashboards.
Click Add .
In the Select - Initial path dialog box, select a dashboard.
Click OK .
Repeat step 7 to 9 to add more dashboards to the slideshow.
Click OK .