Produits : WebStation
Fonctionnalités : Dashboards
Version produit : 2024, 7.0
03/12/2024

Creating a Slideshow

You create a slideshow to automatically switch the display of different dashboards.

Afficher plus
action_close

Slideshows switch the display of several different dashboards or other components. You can configure the interval between the dashboards and components.

To create a slideshow
  1. In WebStation, right-click the folder where you want to create the slideshow.

  2. Click Create Slideshow .

  3. In the Create object - slideshow dialog, in the Name box type a name for the slideshow.

  4. Click OK .

  5. Click Configure .

  6. In the Speed(s) row, enter the interval between dashboards.

  7. Click Add .

  8. In the Select - Initial path dialog box, select a dashboard.

  9. Click OK .

  10. Repeat step 7 to 9 to add more dashboards to the slideshow.

  11. Click OK .

  • How Dashboards Work
  • Slideshow