earth_america
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Пользовательский интерфейс

Пользовательский интерфейс


Продукты: WebStation
Функции: Dashboards
Версия продукта: 7.0
19.12.2024

Dashboard Properties – Basic Tab

Use the Dashboard Properties dialog box to configure a dashboard.

 
action_zoom_plus_stroke Dashboard Properties – Basic tab
Рисунок: Dashboard Properties – Basic tab

Таблица: Dashboard Properties – Basic Tab

Component

Description

Caption

Type a caption for the dashboard.

Show date and time

Select True to display the server date and time in the upper right corner of the dashboard.

Background color

Enter a background color.

Background image

Select a background image.

Blur background

Select True to blur the background image. This will blur the background of widgets if the widget opacity is below 100%.

Opacity

Select the opacity on the widgets.

  • How Dashboards Work