Dashboards are a way to get a graphical overview of values and logs in your system.
You create dashboards to get an overview of how buildings perform, such as energy consumption monitoring, alarm statistics, and environmental summaries. You can view live and historical data.
Dashboards are created in WebStation and can only be accessed through WebStation. You configure the dashboard to your needs by adding dashboards widgets.
Types of Dashboards
There are two types of dashboards, public or personal.
Public dashboards
Public dashboard can be created by any user that has access to the folder where the dashboards are located. Any user that has access to the folder can view the dashboard.
Personal dashboards
Personal dashboards are saved on the user level and can only be accessed by the user that created them. To be able to create personal dashboards, the user must be a member of a that allows members to create dashboards.
For more information, see Allowing a User to Access Personal Dashboards
.
Personal dashboards require a license.
Dashboard Widgets
Dashboard widgets are small applications in a dashboard. Dashboard widgets are the main components in a dashboard and present graphical information from your system.
For more information, see Dashboard Widgets
.
Slideshows
Slideshows switch the display of several different dashboards or other components. You can configure the interval between the dashboards and components.
Dashboards in WorkStation
Dashboard cannot be accessed using WorkStation. However, the dashboard objects are visible in the System Tree in WorkStation.