Dashboard widgets are small applications in a dashboard. Dashboard widgets are the main components in a dashboard and present graphical information from your system.
You can create one or many dashboard widgets in a dashboard. Dashboard widgets can only be created in a dashboard in WebStation.
All dashboard widgets are ready to use. The only thing you have to do is add the trend log or variable you want to display in the dashboard widget. All dashboard widgets have default setting for color and different layout components, but you can also configure them to suit your needs. For example, you can add captions to the widget itself or the x- and y-axis in diagram, you can use different colors for different values or value ranges in a gauge.
Empty space is not a dashboard widget but a way to create empty spaces between dashboard widgets. Empty spaces are used when you do the layout of a dashboard.
A heat map is a graphical representation of data where the values contained in a matrix are represented as colors.
For more information, see Heat Map .
A log pie chart is a circular graphic divided into slices to illustrate proportions of trend logs.
For more information, see Log Pie .
A log value displays one or many trend log values as numerical values.
For more information, see Log Value .
A period chart is used to compare trend logs over different time periods.
For more information, see Period Chart .
A period chart is used to compare trend logs over different time periods.
For more information, see Period over Period Chart .
A point gauge is used to graphically display a current value in a gauge.
For more information, see Point Gauge .
A point pie chart is a circular graphic divided into slices to illustrate proportion of values.
For more information, see Point Pie .
A point value is used to display the present value of one or many variables as a numerical value.
For more information, see Point Value .
A XY plot, also called a scatter plot, is used to display values for two trend logs.
For more information, see XY Plot .
Hyperlinks can also be added to a dashboard. To be able to display the content of the hyperlink, you must enable external content to be embedded in WebStation.
For more information, see Enabling External Content to be Embedded in WebStation .